Problem with compiling in visual coding

Problem with compiling in visual coding

yannic
Established Member

Hello together,

I created a programm in the IDE visual coding. The program works fine. But if the projects gets larger, its not posible to compile it anymore. The IDE don't show a mistake. Whats the problem here? Is there a limit for the size of the program?

Greetings

Yannic

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

There are two possibilities that could cause your problem:

  1. There could be a block used that is not compilable. Are you using any extensions or do you known from the  of which block on it stops working?
    usage
  2. The linting tool could oversee a syntax error and the compiler would crash. Please check this with switching to e.g. JavaScript view and see if errors are shown there.

It would be good for us to check the code you are using. Please send me a private message with your contact data so we can get in direct contact.

 

I found one topic how to break compiling:
If you are using the IPC extension and you added more then one application with the same name there is an ambiguity that the compiler cannot handle. Please check that in the project settings:

2021-07-01_11h07_11.png

2021-07-01_11h07_55.png

2021-07-01_09h47_49.png

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist