FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-30-2023 08:36 AM
Hello everyone,
when I open the PLC Engineering tool in CtrlX Works and open a project, I have to enter an IP-Adress of the CtrlX CORE. When I enter the IP-adress of the ctrlX CORE the connection-test shows a succsessful https request but the PLC isn´t reachable (see picture below).
What could be the problem?
Thank you in advance.
Solved! Go to Solution.
03-30-2023 10:42 AM - edited 03-31-2023 08:32 AM
Could you please tell us which version of the ctrlX CORE system apps, PLC app and ctrlX WORKS you are using?
Is there a ctrlX CORE - PLC app installed on your ctrlX CORE?
03-30-2023 04:46 PM
Yes, there is a PLC App installed. The version of the different Apps isn´t the problem. We tried different versions and currently the 1.18.
For your information: CtrlX Core is running with port fowarding on port 8740.
04-04-2023 09:28 AM
So you are using a ctrlX COREvirtual in port forwarding mode with standard setting 8740:11740.
PLC app version have been different.
Can you please tell us which version of the
04-04-2023 10:10 AM
No, we´re using the CtrlX CORE with port forwarding.
We´re using the Version 1.18 on the System-Apps as well as on the CtrlX WORKS / PLC APP.
04-04-2023 11:12 AM
Could you please tell us which and especially where the port forwarding settings were made in your real ctrlX CORE?
04-04-2023 03:42 PM
The port forwarding settings were made on a switch (Scalance), not on the CtrlX CORE directly. This switch redirects to port 8740.
04-06-2023 04:17 PM
Hi,
can you add a short video here or some screenshots to get an impression how you proceed?
04-11-2023 02:50 PM
Hi @georkueh,
for sure, in the attachement you will find the screenshots how I proceeded.
06-22-2023 11:15 AM
Is this still an issue or can this topic be closed?
06-22-2023 03:03 PM
it is still an issue
06-30-2023 07:16 AM
Hello @jacaré & @CodeShepherd,
with the new CtrlX WORKS update 1.20.2 the problem is fixed.
Thank you.