Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

[Error]CODEMGETCONTENTBYFIRMCODE2 while Using Codesys Add-on Packages

[Error]CODEMGETCONTENTBYFIRMCODE2 while Using Codesys Add-on Packages

soup01Threes
Member

Dear All FA Professional,

I faced an error that while using Codesys Add-on(In my case, Ethernet/IP codesys package is used)

my Ctrlx COREVirtual:1.12.70
my ctrlX WORKS :WRK-V-0112.9
my codesys add-on :4.4.0.0/4.2.0.0

And here is the error outpout in the message window:

[FATAL ERROR] Unresolved reference: 'CODEMGETCONTENTBYFIRMCODE2'
[FATAL ERROR] Unresolved reference: 'CODEMGETCONTENTBYFIRMCODE2'

And this error is shown while I login.

soup01Threes_0-1671788462791.png

I serach from internet and this post have the same issue.
But this post is more 2 years before.
https://developer.community.boschrexroth.com/t5/ctrlX-WORKS/Fail-to-login-the-demo-kit-by-ctrlX-PLC-...

is that any suggestions?

10 REPLIES 10

danielsimila
Established Member

Hi,

This error seems to occur when there is some kind of version-error present between the devices. In the issue you linked there was an issue of combining an older version of the PLC-app on the CORE with a newer version of PLC Enginieering. Which version does your PLC app on the CORE have? If it's not the latest v1.12-version I would try updating to that and see if it solves the issue. 

If you have already tried this I would suggest updating your working environment to v.1.18, if that's possible in your situation.  

Hope that helps, 
Daniel

Hi danielsimila ,

Thanks for your reply!

I try to download the new version , but only 1.12.9 can be download..

 

soup01Threes_0-1672361834144.png

 

And here is my PLC Apps Version

soup01Threes_1-1672361888983.png

 

soup01Threes_2-1672361940511.png

 

Would you please tell me where can i download the lastest version?

 

Thanks,

 

 

 

Open
Occasional Contributor

Dear,

 

Thanks for your reply, But I can not get the lastest version of from your link..
Would I need to send some request first?

Thanks

soup01Threes_0-1672388088210.png

 

Dear soup01Threes,

right now I granted you additional access rights. Please see my e-mail I sent to you.

Regards.

Dear,

After i upgraded the ctlx works to v1.18 and install the PLC apps with -V-0112.5,

This error is shown and warning me that the hardware version and software had problem..

soup01Threes_0-1672830862497.png

 

soup01Threes_0-1672832700095.png

 

 

 

Which image version are you using on your ctrlX COREvirtual now? Are you still on v.1.12 here? 

If you set up a new COREvirtual with v.1.18 image and v.1.18 on the PLC-app, do you still get the error?   

Hallo and thanks for your reply!

I only have the 

I can not download the  v.1.18 PLC-app -  It seems like this version is not released formal.
And i created a vritual-core with v1.18 works.

 

soup01Threes_0-1672840519241.png

 

Ok, I dont know the current state of the release but my belief was that is was officially released. 

But you can not access anything under Home/Ctrlx-Automation/ctrlX_CORE_APPS_Releases/V1.18/ctrlX Apps/DC-APP Paket in the Collaboration Room?

Hi and thanks for your reply!

I found the latest version of PLC apps in that zip file now I can download without error.

 

Thanks for your support;)!!!

 

soup01Threes_0-1672876674937.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist