cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Allocating more resources to CtrlX virtual

Allocating more resources to CtrlX virtual

Anonymous
Not applicable

Being that Ctrlx Virtual is basically a virtual machine, is it possible to provide more processing power to CtrlX? 

Currently, the processing power of the virtual machine is slow and I would like to speed things up by allocating more ram and cores to the virtual machine.

2 REPLIES 2

FooFighter
Established Member

Hello,

Did you make sure that the hardware acceleration works on your computer? If booting the control takes more than one minute, you have to check the hardware acceleration via the i-icon beside the drop down in the extended settings of the control.

It is not (yet) intended to change anything on the RAM via the user interface. Currently you can only do this with QEMU knowledge in a manually edited batch file.

Starting a virtual control in ctrlX WORKS creates always a batch file in the following path '%ProgramData%\Rexroth\ctrlX WORKS\virtual-controls\images\1.10.2\5fgvp1xv.user.qcow2.tap.start.bat'

You can create a copy of this file and edit the ram and cores there (-smp 4 -m 1G) means 4 cores and 1G ram.

Regards

Anonymous
Not applicable

Ahh perfect thank you.

Im running on AMD processor so its HAXM wasnt availble. 

Your answer should work thank you!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist