Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 

Customize the amount of Process Data in SAFEX C.15

Customize the amount of Process Data in SAFEX C.15

nova
New Poster

Hi all!
In the older SafeLogic SLc I could customize input/output process data and I used only 12 input byte/12 output byte (Sercos): for me was sufficent.
Now I have a TwinCat project with only one SAFEX C.15 (EtherCat slave) and in the Process Data obtain already 66 output byte/46 input byte. Is possible customize the process data to reduce exchange input/output bytes?
Thanks in advance.

1 REPLY 1

ctrlXProgrammatore
Long-established Member

Hello @nova ,

The process data is broken up into three sections:

  • FSoE connections (data length depends on number of FSoE devices)
  • Safe-Master-to-Master (SMMC, data length fixed)
  • Functional Data (SAFEX information (status, diagnostics) plus user inputs/outputs to EtherCAT Master, data length fixed)

Here is an example with three FSoE Connections.

  • Slave_Process_Data_Modules = SMMC
  • Slave_Process_Data_Modules_1 = Functional Data

ctrlXProgrammatore_0-1729083720852.png

HTH

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist