Are there other programming languages (like ST) for ctrlX SAFETY than FBD?

Are there other programming languages (like ST) for ctrlX SAFETY than FBD?

AllAutomation
Community Moderator
Community Moderator

The above question arrived out of a discussion with a scandinavian customer.

The answer:

There is only FBD (function block diagram) as programming interface for users. The reasons are

  • Most users ask for safety-certified, ready-to-use function blocks with maximum application-functionality inside, since it is the most efficient way to create applications
  • Function block diagrams are easy to validate and the approval is facilitated

From time to time users ask for more freedom in programming, but this is a request for a specific solution already. We have to understand what's the use case behind that question, to see what we can do to fulfill the actual requirement. Example: It could be motivated by interactive & safe deactivation of maximum application parts, depending on the actual machine configuration.

Please add the use case information here.

BR

The ctrlX SAFETY Team

1 REPLY 1

AllAutomation
Community Moderator
Community Moderator

The answer in the above posting is already given.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist