FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-29-2022 05:48 AM - edited 08-29-2022 05:56 AM
Hello Community,
I am using ctrlX drive demo unit with PLCopen library ladder programming,
When i used MC_Power function block whenever i logged in it will show Error, i tried resetting Warm, Cold and Origin still the same.
But however when i use structured text it has no issue.
Anyone encounter the same issue?
please see attached.
Solved! Go to Solution.
08-31-2022 09:06 AM - edited 08-31-2022 09:27 AM
Which versions of the ctrlX PLC Engineering, CXA_PLCopen library and ctrlX PLC app are you using?
The error tels us that the input is wrong. I can confirm this behaviour (Version 1.12) as long as the AXIS_REF is not set correct. But it is working fine when set correctly:
09-01-2022 04:32 AM
Hello CodeShepherd,
I am using ctrlX PLC version 1.14.1 and CXA_PLCopen library 1.14.0.1
This error only happen sometimes and sometimes after a power cycle it worked normally.
I tried to replicate the error however it works fine now.