10-25-2022 05:12 PM
Hello,
Is the Alarm manager not yet implemented in the Visualization for ctrlX PLC 1.16.1?
Br,
Solved! Go to Solution.
10-26-2022 12:49 PM
To see the "Alarm Manager" in the visu toolbox, you have to add the object "Alarm Configuration"
10-26-2022 01:04 PM
Thanks for your reply - I forgot to mention that I have the alarm configuration in my application.
maybe I should try to reinstall the software?
Br,
10-26-2022 02:08 PM
SOLVED
The solution is not the root-cause of the problem.
I was working with a virtual core. When I change over and work with the real deal the problem disappears.
Br
12-13-2022 08:30 AM
Correct me if I'm wrong but as I tested the alarm manager appeared to the visualization Toolbox only after I added Webvisu to the Visualization manager. Maybe Remote TargetVisu will do the same, didn't test that.
05-29-2024 02:24 AM
Just adding this for my own benefit next time 🙂
The Alarm Manager tab in the Visualization toolbox shows up when you add a WebVisu object under the Visualization Manager.