FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
10-27-2022 12:49 PM
Hello,
We have a ctrlX with the 1.14 version and we have programmed an application with the ctrlX PLC 1.14.1,
The device of the project is a real ctrlX Core with the 1.14 version:
The problem is that everytime we perform the download the system returns an error, it seems that there is a mismatch between the ctrlX Core configured in the project and the real one, however both of them are in the 1.14 version,
Does anyone know why is this happening?
Many thanks,
Solved! Go to Solution.
10-28-2022 02:02 PM
We some more information about what your PLC code is using:
11-02-2022 10:16 AM
Hello CodeSheperd,
We do not use the ctrlX Motion libraries, we have performed a test in an empty project and it seems that there are errors in the following libraries:
If we declare a dtu.GetDateAndTime variable when we compile there are 0 errors (once we install the CAA DUTIL DTU library), however if we download it to the Core the same error appears
We have upgraded the Core to the 1.16 version but still this error pops up,
I attach here also the test program,
11-07-2022 08:58 AM
Hello,
the problem regarding the unresolved externals results from the fact, that the library CAA DTUtils has not been supported with the ctrlX CORE devices. We addressed this issue to our development, but unfortunately it will be RM 23.03 that the bug will be fixed. So please follow the ctrlX CORE release notes!
kind regards