FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
11-02-2023 03:11 PM
Hello,
Our understanding is that the new PLC licensing scheme is based on I/O and tasks in the project, not the target hardware platform. But if I make a new project in ctrlX PLC Engineering 0202.2 and select x64 architecture (for ctrlX CORE X7) it is showing that all 4 PLC license are required, regardless of what's in the application. Only with ARM architecture (for CORE X3) do the required licenses reflect what is used in the project. Is this a case that ctrlX WORKS is not caught up to the new licensing for PLC 02VRS, or is it truly the case that X7 needs all 4 PLC licenses regardless of the application, as with PLC 01VRS?
Best regards,
Brian
Solved! Go to Solution.
11-03-2023 11:26 AM - edited 11-03-2023 11:37 AM
In general the licenses for version 2.x are not longer bound to any hardware.
X64 is not only the system architecture of a ctrlX CORE X7 but also ctrlX COREvirtual and ctrlX CORE OS so the project could be created for several targets and "current required" apps should be wrong visualisation.
I can reproduce the behaviour and we already fixed the bug in in the next release version 2.04 of ctrlX WORKS (including new version of ctrlX PLC Engineering).