Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

No error feedback of drive failure F8022

No error feedback of drive failure F8022

alink
New Contributor

Hello,

how to get an error feedback if failure F8022 (signals incorrect of encoder) occurs in drive?

In ctrlX Drive there is the failure:

alink_0-1682507253631.png

At the same time, in PLC, AxisInfertace, there is NO error:

alink_1-1682507343369.png

No error in ctrlX Core

alink_2-1682507431681.png

alink_3-1682507485119.png

No way to do any reaction to this issue. Any ideas?

8 REPLIES 8

Michael_A
New Contributor

Hello,

in your case you will get an error reaction from motion after you try to switch on the axis with the F8022.
To get more information, independant from motion, you can use the DriveConnect-App.
This will bring you error-messages to the logbook as soon as they appear.

Thanks for feedback. I don't like to use a furhter app.

But I found the status-word P-0-0115 Bit 13 Drive-Error:

0 = no error

1 = error

This is set as soon as there is an issue with engine/drive/feedback -- while PLC / AxisInterface doesn't know anything of that.

CodeShepherd
Community Moderator
Community Moderator

Could you please check behaviour in LTS version 1.20? There as far as I encountered you always get an error message, that drive has an error.

With 1.20 it is still not working, not like it should or known from a MLD-System.

When unplugging an engine from drive, the drive error F8022 occurs in ctrlX Drive

alink_0-1700033871010.png

At the same time in PLC:

axisStatus[x].Diag.Error keeps FALSE

The only way to read out drive error: Parameter P-0-0115, bit 13

alink_1-1700034022265.png

And here, no error as well....

alink_2-1700034250006.png

 

 

CodeShepherd
Community Moderator
Community Moderator

Could please clarify the status of the axis object in the ctrlX MOTION when error occurs? Is it in state "DISABLED" or an active one (e.g. "STANDSTILL")?

It's in "DISABLED".

With the (my) system it must be possible to connect and disconnect engines from drive / PLC while it is shut on, but not while in motion, of course. If an engine is disconnected, then the corresponding drive has to be set to a "parking axis" C1600 / S-0-0139.

The user has to get a message that he know what to do. So therefore the status of an error has to be known, either state is "in motion" or "disabled".

With the former MLD-system the ".diag.error" was used. Now, it is just possible with P-0-0115, bit 13, if engine is not in control.

CodeShepherd
Community Moderator
Community Moderator

Sorry for the late reply tried to get some more information already.

In general you can harm the electronics when disconnecting and connecting devices while powered. 

The current behavior is that the motion will not recognize drive errors when motion object is in state disabled. We are investigating if we change this in one of the next releases but decision was not made until now.

Update: 

the behaviour will be changed from version 2.06 (RM24.03) on.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist