FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-29-2024 07:20 AM
Hello
I'm trying "Fast time series data from ctrlX PLC to local InfluxDB",
download "daq.zip" file,
import this "daq.export" file to CtrlX PLC engineering.
But it can not be imported such like following message.
My current CtrlX PLC engineering information is here.
How do I import "daq.export" file?
Solved! Go to Solution.
01-29-2024 12:44 PM - edited 01-29-2024 12:51 PM
It's possible to edit the *.export file using a text editor, replacing the existing CORE version information with the currently installed target version.
(In my case I have target version 1.20.60.0 installed.)
Since in this case the export file includes the device information, remember to import the resulting export file into the root node of the project.
@jacaré: It might be helpful to include only the Application in the export file:
01-29-2024 02:32 PM
I changed the *.zip-file according to @bostroemc comment. Please download again and try to import.
You need to first select "SPS-Logic" in your project and then "Project" -> "import".
01-30-2024 02:02 AM
Thanks for your information. I did it!