FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
07-20-2023 02:28 PM
Hello,
I have a controller with TwinCAT connected via EtherCAT to a XCS drive. I'm writing in CtrlX PLC Engineering a program with the CtrlX Drive Technology function template which will be downloaded to the drive. I need that this program reads variables from the controller, is there a library with function blocks for ADS read/write operations?
Thanks.
Solved! Go to Solution.
07-20-2023 03:06 PM
Hello MaxS,
As far as I know there is a function to read a parameter from a slave with acyclic communication :
But this one is used as when the CtrlX Core is the Ethercat Master
08-23-2023 09:53 AM - edited 08-23-2023 09:54 AM