01-18-2021 05:26 PM
Hello,
when I try to Launch ctrlX PLC Engineering, I have many times the message error bellow,
I tried to Uninstall/ Install ctrlX Works, the PC, stop all Indraworks services and I have the same issue,
do you have more informations about it ? (All ctrlX Services are launched normally)
Solved! Go to Solution.
01-19-2021 07:03 AM
Hello,
i have the same problem when i am working with a virtual control.
Workaround: 1st start PLC Engineering and 2nd start the virtual control. This works for me.
I entered a bug, so we can hope for a solution.
Best regards,
Klaus
01-20-2021 12:03 PM
Thanks for your feedback,
but in the case we have a PLC Project linked to a ctrlX virtual, we have no way to open it or download it to the virtual control ?
Thanks,
01-21-2021 07:06 AM
Hello,
you have to store the project on your PC.
I think it is possible to work this way:
1. start PLC Engineering without opening a project
2. start virtual control
3. in PLC Engineering, create a new project and select ctrlX COREvirtual
4. in the next dialog select your virtual control and the options you want:
5. I expected to be able to login, but i had to set my communication parameters here:
Now you should be able to login.
Next time just open the project from the PC.
Best regards,
Klaus