07-08-2022 10:26 AM
Hi,
Shall we control a servo motor directly by only using PLC app with "PLC Open" library without using Motion App?
If yes then could you tell me how to declare the Axis variable as attched picture?
Thank you!
Solved! Go to Solution.
07-08-2022 11:09 AM
When drives only are connected as an IO you cannot use the standard motion function blocks like MC_Power. These are interfaces to the motion runtime. You will have to handle the control and status word as well as the set frequency/speed by hand.
07-12-2022 09:27 AM - edited 07-13-2022 09:54 AM
Every Function block in PLCOpen library will use infrastructure of app.motion. So CXA_PLCOPEN can not work without app.motion.
07-13-2022 04:12 AM
07-13-2022 09:56 AM
Sorry I made a typing error😓. I mean CXA_PLCOPEN can not work without app.motion.
07-13-2022 10:09 AM
No problem!
Thank you for your all support!
Br,
07-13-2022 10:40 AM - edited 07-13-2022 10:42 AM
Hi, guys
If so, I can't use PLCopen Library in EtherCAT CoE protocol (3rd party drives) without motion app?
I have to control more than 30 axes with 3rd party drives.
07-13-2022 12:14 PM
Yes, for PLCopen Motion library you need ctrlX MOTION. With RM22.11 (V1.18) in November 2022 we plant to support more than 30 axes with ctrlX CORE X7. Conccerning further details, please give me a personal note PN.