Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Unable to reset axis error

Unable to reset axis error

JHU1XI1
Long-established Member

Hello,

MC_ReadStatus.Errorstop :=true; At this time, it is not possible to reset through the reset function block,

if MC_ Reset.Execute=True Then

MC_ Reset will output error.

After power outage and restart, everything is normal.

2023-09-14_09h36_13.png

2023-09-25_11h31_24.png

 

4 REPLIES 4

CodeShepherd
Community Moderator
Community Moderator

Could you add some more information?

  • What is the active command for "Axis_2" before error occurs?
  • Which error is occurring?
  • Could you switch on motion traces and create a system report after while the state you are showing is active? (Check out this post for how to do so)

JHU1XI1
Long-established Member

When two axes are running in gantry mode, the enable suddenly disconnects, and at this time, the axis reports ErrorStop, with one driver displaying Ab and the other displaying AF, which cannot be reset.

This phenomenon does not always occur, and may occur after a period of time. I will follow your method to obtain more information.

JHU1XI1
Long-established Member

When two axes are running in gantry mode, the enable suddenly disconnects, and at this time, the axis reports ErrorStop, with one driver displaying Ab and the other displaying AF, which cannot be reset.

Collect information according to your guidance.

2023-10-18_11h27_54.png

CodeShepherd
Community Moderator
Community Moderator

As you are using an outdated version 1.18 of the installed apps please update to current long term service release 1.20 and test if error is still occurring.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist