cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Third party drives( CoE protocol)

Third party drives( CoE protocol)

PlamNi
New Poster

Hallo,

I am trying to to configurate third party EtherCat servo drive which support CiA402 profile to work in MOTION application.I have installed MOTION app version 1.14,PLC,ETHERCAT applications and I have set several attributes:scalingStrategy-COE_CALC_CONTROL, scalingType- LINEAR,numerator-1000, denominator-1000,resolution-4000. When i have run "Motion operation mode" , the following error appears "091F0004 AxisProfile state machine errorSwitch statemachine to Running failed". Can you please suggest me a solution to the error?

Thank You in adwance!

6 REPLIES 6

LuisCtrL
Established Member

Hello,

Probably it could be the XML file which is loaded into the CtrlX IO Engineering.

Could you share pictures of the configuration of the slave? Maybe there is some incompatibility.

 I have tested this .hml file on a Beckhoff PLC and everything works. Now I tried to run another  servo motor with CtrX plc and it gives the same error. I am sharing pictures of slave axle settings.

Sharing more pictures of the slave axis settings.

CodeShepherd
Community Moderator
Community Moderator

Sorry for the late reply. Could you send me a private message with your contact data so we could have a direct look to it?

This is of interest to me as well - I'm bench-testing a Core X3 with one of our standard machines that uses Omron today. 

I have more or less the exact problem but with an Omron Serv

Br,

CodeShepherd
Community Moderator
Community Moderator

Could you please have a look to this thread for further information?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist