FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-21-2022 02:32 PM
Hallo,
I am trying to to configurate third party EtherCat servo drive which support CiA402 profile to work in MOTION application.I have installed MOTION app version 1.14,PLC,ETHERCAT applications and I have set several attributes:scalingStrategy-COE_CALC_CONTROL, scalingType- LINEAR,numerator-1000, denominator-1000,resolution-4000. When i have run "Motion operation mode" , the following error appears "091F0004 AxisProfile state machine errorSwitch statemachine to Running failed". Can you please suggest me a solution to the error?
Thank You in adwance!
Solved! Go to Solution.
10-27-2022 11:55 AM
Hello,
Probably it could be the XML file which is loaded into the CtrlX IO Engineering.
Could you share pictures of the configuration of the slave? Maybe there is some incompatibility.
10-28-2022 04:18 PM
10-28-2022 04:22 PM
11-15-2022 07:25 AM - edited 11-15-2022 07:25 AM
Sorry for the late reply. Could you send me a private message with your contact data so we could have a direct look to it?
11-16-2022 03:33 PM
This is of interest to me as well - I'm bench-testing a Core X3 with one of our standard machines that uses Omron today.
I have more or less the exact problem but with an Omron Serv
Br,
11-22-2022 10:24 AM
Could you please have a look to this thread for further information?