FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-14-2024 10:43 AM
Hello,
I have 11 axes and ctrlX Core X7 and I have declared correctly the 11 axes in the ctrlX Motion app,
The problem seems that in the ctrlX PLC Environment I cannot use more than 10 axis,
I am using the version ctrlX PLC 1.20 and if I try to modify this value is blocked because It is embedded in a library of the PLC
How can I change this? If I cannot can I command more than 10 axes in the ctrlX PLC with the ctrlX Motion?
Thanks,
Solved! Go to Solution.
03-14-2024 10:59 AM - edited 03-14-2024 10:59 AM
The allowed range is up to 63 axis. The configuration dialogue needs to be used:
ctrlX PLC Engineering - CXA_MotionInterfacUser - configuration