FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-27-2024 03:56 AM
Hello,
Can we use the gantry function in the Motion App to synchronise multiple hydraulic axes (ex: IAC - 4WRPDH)? Also to rephrase the question, is it planned for ctrlX to have something like the MLC for hydraulic drives?
Thanks.
Solved! Go to Solution.
02-27-2024 07:26 AM
Please have a look to the "Bosch Rexroth - H4U.app xF - position force control" and the "Bosch Rexroth - H4U.app pQ - pressure flow control". I will check if there are further information corresponding to your case.
02-29-2024 10:48 AM
The 1st hydraulic controller which will be available for the ctrlX-plattform will be the pos/force controller. It will be provided as PLC-lib. The release is planed for end of march 2024, being published in the STORE.
The experience regarding expected performance on ctrlX Core as well as on hydraulic-axis side are restricted right now, since we await the release as well.
You mention the sychronious control of several hydraulic axis. Well, the "Gleichlaufregler'/Sync-Controller" like known from the MLCH controller will not be available by then. I expected there releases afterwards, but the timeline is not predictable so far.
Depending on the application-requirements it may be worth to check if the hydraulic axis could be coupled with the motion-app provided synchronious features.
As soon as the release is published we will start working with it.
05-09-2024 08:21 PM
09-06-2024 12:18 PM - edited 09-06-2024 12:34 PM
Hello team,
Is the PLC lib available for control of position/force for hydraulic motion in the core? is this same as H4U app but for xF?
Thank you
09-18-2024 03:58 PM
Hello Tasty_Tech,
please check your incoming Messages and respond with an email, because h4u provides the pos/force controller for testing under trial-license.
The plc-Lib will be send by the hydr. colleagues.
Please feel free to demand for p/Q and Synchronization axis as well directly at the h4u team.
Bye
09-19-2024 08:06 AM
One thing to consider is that the HMC should work out of the box with ctrlX MOTION (Its based on a IndraDrive Cs), and that can do all syncronisation and other stuff. And there's no performance limitations in the same way as the PLC based one (ie 10 axis on a X3 will be fine).