Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Motion FlexProfile

Motion FlexProfile

DCEN_Tony
Established Member

Hello,

I have some basic queries about what I need to use Motion FlexProfile on Ctrlx Core in Drive:

1. I believe I need the Motion Electronic Gear add-on (R911417992), Motion FlexProfile add-on (R911417994) and PC Cam Designer (R911421308). Do I also need the CODESYS - Softmotion add-on (R911411672) or is the CODESYS Softmotion (used for electronic cams etc) independent to the Motion FlexProfile handling?

2. Is Motion FlexProfile supported with the 1.20 apps / CtrlX Works or do you need to use >=2.02?

Many thanks

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

To be technical able to use the camming function of the ctrlX MOTION you need to have this app and the ctrlX CORE system on version >=2.02. So access to pre-release area on the collaboration room is needed.

And following licenses:

  1. ctrlX OS License - Motion Standard 4 Axes R911400503 - SWL-XC*-MOT-STDMOTION****-NNNN (or ctrlX OS License - Motion Standard 10 Axes
    R911414460 - SWL-XC*-MOT-STDMOTION**10-NNNN)
  2. Additionally ADD-ON ELECTRONIC GEAR R911417992 - SWL-XC*-MOT-ELECGEAR*****-NNNN
  3. Additionally ADD-ON CAMMING R911417993 - SWL-XC*-MOT-CAM**********-NNNN
  4. Additionally ADD-ON FLEXPROFILE R911417994 - SWL-XC*-MOT-FLEXPROFILE**-NNNN

CAM Designer (licence needed: R911421308 - SWL-PC*-MOT-CAMDESIGNER**-NNNN) is optional, as the flex profiles can also be created via REST or PLC.

The CODESYS Softmotion is totally independent of the ctrlX MOTION and so not needed.

Thanks for the quick reply.

To note I could not see an option for ADD-ON CAMMING R911417993 - SWL-XC*-MOT-CAM**********-NNNN in the configurator or referenced as a requirement in any Release Milestone presentations

As this license was added just recently, it will be added to the ctrlX Configurator in one of the next updates.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist