09-29-2023 12:23 PM
Hello,
I have some basic queries about what I need to use Motion FlexProfile on Ctrlx Core in Drive:
1. I believe I need the Motion Electronic Gear add-on (R911417992), Motion FlexProfile add-on (R911417994) and PC Cam Designer (R911421308). Do I also need the CODESYS - Softmotion add-on (R911411672) or is the CODESYS Softmotion (used for electronic cams etc) independent to the Motion FlexProfile handling?
2. Is Motion FlexProfile supported with the 1.20 apps / CtrlX Works or do you need to use >=2.02?
Many thanks
Solved! Go to Solution.
09-29-2023 06:29 PM - edited 10-02-2023 11:47 AM
To be technical able to use the camming function of the ctrlX MOTION you need to have this app and the ctrlX CORE system on version >=2.02. So access to pre-release area on the collaboration room is needed.
And following licenses:
CAM Designer (licence needed: R911421308 - SWL-PC*-MOT-CAMDESIGNER**-NNNN) is optional, as the flex profiles can also be created via REST or PLC.
The CODESYS Softmotion is totally independent of the ctrlX MOTION and so not needed.
10-02-2023 09:43 AM
Thanks for the quick reply.
To note I could not see an option for ADD-ON CAMMING R911417993 - SWL-XC*-MOT-CAM**********-NNNN in the configurator or referenced as a requirement in any Release Milestone presentations
10-02-2023 11:46 AM
As this license was added just recently, it will be added to the ctrlX Configurator in one of the next updates.