02-08-2024 02:51 PM
Hello
We have Indradrive CS and configured it with Motion 1.20.8 and CtrlX Core 1.20.12
We have problem with clearing Emergency-stop error, while axis is in ModeAB. We also don't see error on CtrlX.
We tried clearing with commands:
Solved! Go to Solution.
02-09-2024 08:49 AM - edited 02-09-2024 09:05 AM
Please check topic "No error feedback of drive failure F8022" as base is similar. In short drive errors are not recognized by the ctrlX MOTION when motion object (axis) is in Ab. This will change in version 2.6.
So currently the MotionInterface does ignore the clear error bit, as using reset error function on a drive without having an error (being in state error) is a violation of its state machine. Also there is an extension from 2.4 on that in Disabled and Standstill the function can always be executed.