FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-20-2021 11:38 AM
Hello,
I'm trying to configure an axis in a new virtual machine created with Ctrl Works 1.10.3 but I could not switch the motion from configuration to operation. Attached you have the configuration I did and the messages I get.
If I start an old virtual machine made with CtrlX Works version 1.6 it works
Please could you help to to understand why?
Many Thanks
Giuseppe
Solved! Go to Solution.
07-22-2021 07:57 AM
This is mostly caused by missing callables in the scheduler (especially the motion callable in ctrlXAutomation task).
If you create a new virtual control there are some files in the configuration that prevent creation of these callables.
To solve this issue you can use the reset function to create an empty solution in “Manage app data” (attention: your changes are lost). The necessary tasks and callables will be created correctly. But you should stop your schedule before …
After that the missing callables should be available.
07-22-2021 08:55 AM
Hello,
I tried to do what you suggest but I got and error while doing the Reset command. I tried it on the Virtual Machine I had and I got the 1st errors, then I deleted that virtual machine and create a new one and then tried again to to the Reset command but I got a different error. However in bith case it was not possible to end the Reset command.
Any other advice ?
Many Thanks
Giuseppe
07-22-2021 10:42 AM - edited 07-22-2021 10:49 AM
The motion and the sceduler should be stopped before resetting.
motion state --> CONFIGURATION
scheduler state --> CONFIG
Which version of motion app do you use?
07-22-2021 11:12 AM
Hi,
I did not stop the scheduler before. Now I tried it again and the Reset command was OK and after that it was also possible to switch the motion to operating mode
Many Thanks
Giuseppe
08-03-2021 09:53 AM - edited 08-25-2021 10:38 AM
EDIT: When getting the error "Error in system configuration - 091F2020 and sub code 0C56020E":
You do not need to reset your AppData (active configuration). You can also simply add a new task in the scheduler and inster the new callable "motion-high-prio-prep":
08-24-2021 02:33 PM
I had the same problem when I upgeaded to 21.07 but the diagnostic ID I got did not come up when I searched for it. So I'm adding it here.
I got "Error in system configuration - 091F2020 and sub code 0C56020E
08-25-2021 10:38 AM
Thanks for the addition.