cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Cannot switch to "Running" configuring a ctrlX Drive in CoE with FSoE

Cannot switch to "Running" configuring a ctrlX Drive in CoE with FSoE

ericvergara
Occasional Contributor

Hello,

I am trying to command a ctrlX Drive throught CoE and with FSoE with a ctrlX Core X7 V2.6 and I have also plugged a SAFEXC15 as a FSoE Master,

I have configured the drive in modulo but the problem is that if try to switch to "Running" the system does not allow me and two errors appears,

ericvergara_0-1721653393222.png

 

I do not know how to create this "axisprofile" task and I have configured the axis in this way,

ericvergara_1-1721653453172.png

ericvergara_2-1721653500149.png

What should I do?

Thank you,

7 REPLIES 7

EngJay
Long-established Member

Which firmware version are you using in the ctrlX DRIVE?

ericvergara
Occasional Contributor

Hello, FW 0504

ericvergara_0-1721717761944.png

 

Michael_A
New Contributor

Hello, can you provide a systemreport of your control with the active app data included.

In case of a SAFEX in your project it could be a problem with the configuration. In this case you can see it on ethercat. If one devices doesn't go to OP there could be a problem with the FSoE connections.

Michael_A
New Contributor

Michael_A_0-1721733826510.png

so can you check this parameter and set it to -1

 

ericvergara
Occasional Contributor

Hello Michael_A,

I have already changed this parameter but now I am getting this error:

ericvergara_0-1721889446341.png

All the devices seem to be in OP

ericvergara_1-1721889617834.png

I attach the system report,

Are there any news? is this still a problem?

This problem can appear when the IO configuration was changed while machine is running. You have to switch the ctrlX MOTION to configuration and back to operating or reboot the control.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist