04-13-2021 09:58 AM
I have tried to connect an Ethercat I/O S20-EC-BK with a Digital Input Device S20-DI-16/1. I can get it to connect and running properly on the core with ctrlX I/O engineering.
However I would like to add virtual Axes after in order to control them with inputs from the Digital I/O Device. I can add the Axes in the Motion Configuration tab, however as soon as I would like to switch the Motion to Run, I get the error message Axis profile is booting and then the Motion switches back to configuration mode.
Same if I try to go to TIGER and would like to initialize the motion it gets stuck on the switching to running mode screen.
Thanks for your help
Solved! Go to Solution.
04-13-2021 11:33 AM - edited 04-13-2021 11:34 AM
Did you add any AxisProfiles to your system? This would only necessary if real drives are connected.
Does the EtherCat boot up to OP?
Which errors are shown in the diagnostic log?
We could have a online meeting to have a look to it. Please send me a private message including your contact E-Mail address.
04-13-2021 12:32 PM - edited 09-10-2021 02:32 PM
As I heard the problem could not be reproduced any more. So please get in touch with us again if there are further topics.