10-18-2022 05:45 AM - edited 10-18-2022 05:48 AM
I try to connecting IndraDrive MPB and IndraDrive MPE servo drive, but it will show switching profile failed.
If I removed IndraDrive MPE, it will no more error.
Delete the Drive MPE, and no more error.
Have I missed some settings?
core version is 1.14.0
Thank you.
Solved! Go to Solution.
10-18-2022 07:08 AM
We had this problem too to resolve this we upgraded our ctrlX system image and motion app to v1.16.
10-19-2022 07:47 AM
Hello,
this was a missing feature up to V1.14 (RM22.03). With V1.16 (RM22.07) you can also add IndraDrive Economy (MPE firmware) to ctrlX MOTION. I added the tag "mpe" here to this topic. If you click on this tag you will find the thread with all the details "AxisProfile error after update to RM22.03"
10-24-2022 09:31 AM
I see. Thanks for all helping reply!
I will try to update.