FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
08-10-2023 02:19 AM
Hello,
I understand the PR21.2 was due to be released in July, is it ready for order yet?
Also it was mentioned in RM23.03 that it is Windows 11 ready, does this mean we can install any Windows based software (ex: ctrlX Drive Engineering)?
Thanks
Solved! Go to Solution.
08-10-2023 09:58 AM - edited 08-10-2023 09:59 AM
Hi Tamer,
we modified it a bit and therefore the schedule is not september it will be december. Perhaps its also interesting for you that we will have not only one variant we will have two: PR21.2 and PR22.2
PR21.2
- is the successor product of PR21.1 and due to the updated components it has a ~9 times better perfromance (CPU benchmark)
PR22.2
- is like the PR21.2 but with additional perfromance increase, more RAM and memory.
Win11 ready means that the hardware is able to run it. So far Microsoft did not release the Win11 version for IPCs. As soon as we have it we can test it.