12-21-2023 08:21 AM
We want to connect the external monitor to ctrlX as the same as PR21 to show the dash board after all of setting finished. How to do it?
Solved! Go to Solution.
12-21-2023 03:04 PM
Hello @taka_urai ,
Since ctrlX OS is providing a web server, any networked device should be able to display web pages from the ctrlX device.
Could you please explain a little more what you are trying to do?
If it is just accessing the ctrlX OS web interface, you can simply enter the ip address of the ctrlX device into a browser on the external device. You can try this on your smartphone after placing the ctrlX device on a wifi network and connecting your smartphone to the same network.
12-22-2023 12:39 AM
Hello Sgilk-san,
Thank you for your advice.
We will make the dash board by NodRED in ctrlX, and we want to see this dash board on the external monitor which is connected to ctrlX by wired (USB?). Do we need somthing to set up? Please advice.
12-27-2023 11:21 AM
Hello,
There is currently no way to do what you're asking for. you need a tablet or a web HMI (we have also) to display a dashboard.
Probably there will be the possibility (still on decision) with the x5 or x7 to display a web browser trough the displayport.
Still on mybe anyway, youi have no choiche than use a webHMI
Mauro
09-06-2024 01:44 PM
As additional information for X5 and X7 there is a an display app available now to show visualizations via the available display port.