Using Terminal to run Node.js command

Using Terminal to run Node.js command

Bala
Member

Hello,

I am having an issue with a 3rd party node in Node-Red and there's a resolution for it on the github forum but I do not know how to implement it. I will need to run the following command: export NODE_OPTIONS=--openssl-legacy-provider but am not sure how and where to run it from. I usually run such commands from the terminal if Node-Red is installed locally on PC but can't seem to figure out how to do it here. Any help on this is appreciated.

Thanks,

Bala

3 REPLIES 3

Sgilk
Frequent Contributor

Hi @Bala ,

Since there is no terminal within Node-RED, you'd have to do this over SSH. You could also build the node offline, include the necessary configuration, package it as tar.gz, and then install the package manually in Node-RED.

Which pallet are you trying to work with? Is this on a physical or virtual CORE?

Hi @Sgilk ,

I am working with the opc-da-in pallette (https://flows.nodered.org/node/node-red-contrib-opc-da). This is on physical core X3. Any documentation on how it can be done over SSH? My knowledge is limited when it comes to building node offline.

Sgilk
Frequent Contributor

On a physical CORE, you'll need to request an ssh user assertion. This would not be valid for a production solution and only for development purposes.

See this How-To for more info.

If exporting the environment variable is required and you don't have ssh access, I think your best bet will be building a custom Node-RED snap.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist