07-09-2024 12:05 PM - edited 07-09-2024 12:19 PM
I am using Telegraf to send a measurement ("Test1") to InfluxDB. Currently, I have two fields read from DataLayer nodes: "Value" & "Timestamp".
Configuration:
[[inputs.ctrlx_datalayer.subscription]]
measurement="Test1"
[inputs.ctrlx_datalayer.subscription.tags]
SensorNum="Sensor1"
[[inputs.ctrlx_datalayer.subscription.nodes]]
name ="Value"
address="plc/app/Application/sym/GVL/Sensor1/Value"
[[inputs.ctrlx_datalayer.subscription.nodes]]
name ="Timestamp"
address="plc/app/Application/sym/GVL/Sensor1/PLCTimeStamp"
Example of the DataLayer nodes:
"plc/app/Application/sym/GVL/Sensor1/Value" : 20
"plc/app/Application/sym/GVL/Sensor1/PLCTimeStamp" : 1720520212398
The PLC variable "PLCTimeStamp" is a timestamp in milliseconds. Instead of providing it as a field, I wanted to provide it as an InfluxDB timestamp. Is this possible using Telegraf?
Thanks in advance 🙂
Solved! Go to Solution.
07-09-2024 02:34 PM
Hi @star_board
in Telegraf you can either use aggregators an processors to transform your data. See the Telegraf manual for more information: Transform data with aggregator and processor plugins
I have not tested for your specific usecase but I found three plugins which could maybe help you:
Best regards,
Nick
07-09-2024 07:19 PM - edited 07-09-2024 07:33 PM
Is there anyway where I can save/see the ouput metrics of telegraf (besides influxdb) in order to test this different plugins?
Would something using an ouput plugin work on ctrlX, like File Ouput Plugin ?
[[outputs.file]]
files = ["stdout", "/tmp/metrics.out"]
data_format = "influx"
07-09-2024 11:25 PM - edited 07-09-2024 11:28 PM
Hi @star_board ,
Something like this should work for your use case, utilizing the Starlark processor @nickH mentioned.
[[outputs.influxdb_v2]]
urls = ["https://127.0.0.1/influxdb"]
token = "eaN73XZ4kWNzTwqkzWrhJpcH2ZJsZjkzuRwOPl-fe0cNMrMrg-2yRoJQvMYpnMVzBxLa8GN6EcXx42JEnEU2w="
organization = "boschrexroth"
bucket = "boschrexroth"
insecure_skip_verify = true
## Configure the input plugin with the username and password to ctrlX Core
[[inputs.ctrlx_datalayer]]
server = "localhost"
## Authentication credentials
username = "boschrexroth"
password = "boschrexroth"
## Use TLS but skip chain & host verification
insecure_skip_verify = true
[[inputs.ctrlx_datalayer.subscription]]
measurement = "metrics"
nodes=[
{name="cpu_usage_percent", address="framework/metrics/system/cpu-utilisation-percent"},
{name ="timestamp",address="system/info/time"}
]
## The switch "output_json_string" enables output of the measurement as json.
## That way it can be used in in a subsequent processor plugin, e.g. "Starlark Processor Plugin".
output_json_string = false
[[processors.starlark]]
source = '''
load("logging.star","log")
def apply(metric):
log.error("----------------------")
log.error(metric.tags['node'])
if "timestamp" in metric.fields:
log.error("Timestamp old: " + str(metric.time))
metric.time = metric.fields['timestamp']
log.error("Timestamp new: " + str(metric.time))
return metric
'''
In the starlark processor, you would look for your PLCTimeStamp field and set the metric.time to that value. Here I used the time coming from the ctrlX system.
07-09-2024 11:31 PM
Yes, the File Output Plugin is supported. You can view a full list of supported plugins on the Github.
07-11-2024 09:38 AM
If I use the File Output Plugin where can I save the output file? And how can I access it?
07-11-2024 05:36 PM - edited 07-11-2024 05:43 PM
You can write to the active configuration. USB access is currently not supported, but I requested this for a future release.
Example:
# Send telegraf metrics to file(s)
[[outputs.file]]
## Files to write to, "stdout" is a specially handled file.
files = ["/var/snap/rexroth-solutions/common/solutions/activeConfiguration/telegraf/test.out"]
data_format = "influx"
You can then access the file in the active configuration Web UI or via WebDAV.
07-11-2024 05:50 PM - edited 07-11-2024 11:06 PM
Thanks for the help! I did manage to do it using your example with starlark processor! 😁
I had to slightly modify my approach and store the variables "Value" and "PLCTimeStamp" in a DataLayer array, rather than in separate nodes, to retrieve them in the same metric instance:
[[processors.starlark]]
source = '''
def apply(metric):
metric.time = int(metric.fields["PLCTimestamp"])
return metric
'''
Additionally, I experimented with using the Converter processor. I will leave the code here since it might be usefull to another person:
[[processors.converter]]
[processors.converter.fields]
timestamp = ["PLCTimestamp"]
timestamp_format = "unix_ms"