Node Red - Deploy error after Subscription update

Node Red - Deploy error after Subscription update

E_Stapel
Long-established Member

Hello everyone,

I had the problem that the Node Red Server lost the connection as soon as I want to read data of the OPC UA Client with the Subscription Node.

Because of that I updated the Subscription Node to its latest Version (1.9.5). I use the CtrlX V1.20 and the Node Red Version 1.20.0+3.0.2-ctrlx.

Since I made this update I can´t depoly anymore. I recive the following error message:

E_Stapel_0-1711381370821.png

On the device is enough storage free.

Does anybody knows this kind of error message / problem?

Thanks in advance.

4 REPLIES 4

Sgilk
Frequent Contributor

Hi @E_Stapel ,

The error message is saying there is not enough free space to deploy the changes to the flow.

What other applications are installed on the device?

Are you able to deploy changes that do not include the subscription node?

E_Stapel
Long-established Member

Hello Sgilk,
I checked my storage space again and actually there is so more space left.
Yes, I can´t deploy other Applications without the subscription Node. So the problem should not be the subscriptin node...I have to check why the storage is full.

Thank you. 

MauroRiboniMX
Contributor

Hello @E_Stapel,

Seems that you need a clean start, reset the actual configuration 🙂 . Plus in these days we're moving to the next version the 2.6 that will be the official LTS in July.
If the machine is going to be in production later than July consider to update to 2.6 🙂

@E_Stapel Are there any news? Could this issue been solved?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist