01-16-2023 01:12 PM
Hallo,
i have installed the InfluxDB APP on the ctrlX Core. The data is send to the database via Device Bridge.
Now I want to export the data stored in the InfluxDB to process it on another device.
The best variant would be to be able to save the data in a csv file.
How can the data be exported from the InfluxDB on the ctrlX Core?
Solved! Go to Solution.
01-17-2023 04:19 PM
That's the solution:
1.
2.
01-18-2023 09:32 AM
Hi,
Yes, then depends on what is the goal! if you want to do it sitematically then it is better to setup something with node-red or python and be sure not to request too much data!
Generate CSV output : Node-RED (nodered.org)
Mauro