FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-19-2022 03:53 PM - edited 10-19-2022 03:54 PM
Hello to everyone,
Today i tried to run the ctrlX i/o s with a potential customer which has Omron as master ethercat but we were not able to run them. He expected to write the address and then reboot the IOs but it fails during the address writing process. the error states in italian: "impossible to set the slaves addresses"
Is there already someone who tried them with Omron or encountered a similar issue?
Mauro
Solved! Go to Solution.
10-20-2022 04:56 PM
We're in clarification and will inform on news.
10-24-2022 08:20 AM - edited 10-25-2022 02:06 PM
Omron control currently not supported, because the Station Alias Register 0x0012 is 0.
The ctrlX IO are developed to support ctlrX CORE in the first step. The implicit addressing with the ctrlX CORE works fine.
We are checking for improvements with future releases.
05-22-2024 02:09 PM
Hello,
This problem is solwed at this time or not?
Regards, Antal
05-22-2024 07:58 PM
Hello Mauro,
Yes I have same problem now.
When I make a firmware update to 1.4.0 on the XC-EC-12, the ethercat coupler is working fine, but the XI110116 Input and+or the XI211116 Output modul is the next, that have problem with the node address.
Somebody has a solution to this problem?
Anti