12-08-2023 10:50 AM - edited 12-08-2023 11:06 AM
I have a yellow led blinking on my Output module XI432204 (0 .. 20 mA) Even if it is not connected. (for me not connected = 0 mA.... and that do not have to give problems) Effected units on my side: XI432204 and also XI442204
Checking the datalayer on XI432204 and also XI442204 shows me the cause : Wirebreak
Solved! Go to Solution.
12-08-2023 10:59 AM - edited 12-08-2023 11:07 AM
Checking the firmware I found that this were very early bought hardware modules.
Firmware on both module was 1.0.2 (old) I updated this with the new firmware from the website. 1.2.0 Now the "problem" is Gone/Solved.
But beware: Module XI442204 is a 4..20mA unit. Not connected is 0 mA and not 4 mA, So then ofcause you still have wire break....