cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

I/O Link Slave - I/O Engineering

I/O Link Slave - I/O Engineering

rum1
Established Member

Hello all,

I would like to connect several Beckhoff IO-Link devices via the ctrlX I/O Engineering. However, I have not found a way to install the IO slave files. 
Attached are the error messages.

3 REPLIES 3

cc2go
Occasional Contributor

Hello,

Currently this kind of Beckhoff devices, which need additional IO-Link configuration support in the tool, isn't supported.

Currently no IODD support by IO Engineering.

We recommend to use an ESI based IO-Link Master Gateway, like they are offered by ifm.

Hello @cc2go ,

and if I would use an IO-Link Master from IFM (which ctrlX supports) and connect a Beckhoff module with only IODDS support (e.g. epi2339 ) , would it work then ?

Regards, Stefan

cc2go
Occasional Contributor

This will work, but the IODD support is with the IFM tool, like Moneo or LR Device, only

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist