cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

EtherCat Modul Adjust parameters

EtherCat Modul Adjust parameters

Engi
Member

Hello,

i´m using the S20_EC_BK Ethercat Fieldbus coupler with an S20-AI-4-UTH to read the values of an Thermocouple Type K.
Now i need to change the parameterizion of the UTH-module.

How can i achieve this via the ctrlX I/O.

Thanks in advance.

 

2 REPLIES 2

cc2go
Occasional Contributor

Hello,

two possibilities, to configure the module

  • ctrlX I/O Engineering with the "Startup Parameters" on the S20-EC-BK, it's explained in chapter 7 "Startup parameterization" of S20-EC-BK docu R911385711_02.pdf
  • use of the PLC library CXA_S20 (available with v1.8.0 or newer)

Thanks a lot for the fast answer.
It’s working now perfectly.
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist