CtrlX-Core and Keyence Stepper Motors

CtrlX-Core and Keyence Stepper Motors

GustavoTaffarello
Established Member

Hello folks,

Just wondering here if it is possible to have the CtrlX-Core controlling a Keyence Stepper Drive. The drive model is QS-10P and the motor model is QS-M60.

My concern here is if it is possible to use the S20-PWM modules connected beside a S20-EtherCAT bus coupler. Having the CtrlX-Core as EtherCAT master here.

If the S20-PWM does not work, another approach would be having the CtrlX-Core as Profinet master controlling a R-IB IL Profinet bus coupler and the R-IB IL-PWM module.

My oher concern would be the RIL_InlineIOModule library, is it possible to install it in the CtrlX-Core?

Which way should I go here?

I have also added this question in the Controls Forum thread below:

https://connect.bosch.com/forums/html/threadTopic?id=a2d9e723-d3e5-4015-91fb-44feea69588a

Thanks a lot.

1 REPLY 1

CodeShepherd
Community Moderator
Community Moderator

Please see this topic for which S20 modules can be used at ctrlX CORE with S20-EC bus coupler.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist