Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Static IP address WR21 WebPanel

Static IP address WR21 WebPanel

V_A
Long-established Member

Hello,
I am not able to assign a static IP address to my WebPanel WR21. I tried to set the IP address in the setting of "Network and internet". After tapping on "Ethernet" and "Setting Ethernet" I can turn on the switch of "use static settings" and fill in the IP adress and the subnet mask. Trying to save the change, a massage appears on the bottom with the massage "Networkinformation is not complete, please fill in the complete". In my case there is no gateway and also no domain1 or domain2. 

How can I assign a static IP address to an WR21 WebPanel?

4 REPLIES 4

Open
Occasional Contributor

Hello V_A,

Try assigning ip address to ETH1 and connect your network cable to ETH2 in WR21.

interface of ethernet 1 and 2 are interchanged.

Ethernet 1 is XETH2, Ethernet 2 is XETH1

See this.

V_A
Long-established Member

Hello Open,

thanks for the answer. I tried this already, but it wasn't a solution in my case.

Attached are some pictures of my input and the massage below.

maurusbien
Established Member

Hello V_A,

Did you tried to fill in every option of an adapter configuration even if you do not need it? (e.g. gateway, domain 1 and domain 2 of picture Eingabe.jpg) Even if this is not needed or used, the system needs it so save the settings...

V_A
Long-established Member

Hello Maurusbien,

thanks for your answer it is also the solution. My mistake was the wrong formate of the domain1. The write formate is for exampe "1.1.1.1". The Problem is now solved.

Thank you.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist