Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with WebIQ Trend on WR21

Problem with WebIQ Trend on WR21

TiborZ
New Poster

Hello,

I have the issue that WebIQ Trends showing up different on two different devices. The server runs on a CORE X3. On the picture attached I had connected a laptop (the trends look how they should) and a WR2110 (the trends look faulty).

On the WR21, the trends are not shown historically but show the actual values over the complete time interval (e.g. 1 minute, no affect of changing the interval).

There is a different behaviour in some other points too:

When unchecking and re-checking some trends via the Trens Select on both devices, the y-axes are grouped the way initially defined only on the laptop, not on the WR21.

In case I only selcet one trend to be shown, the laptop shows one fixed y-axis and the moving trend. On the WR21 the trend remains in the middle of the widget and the y-axis is moving instead.

 

Setup:

X3 with 1.20, WR2110 RC7, WebIQ 2.15.7 (both, designer and server).

The devices are offline but time is synchronised (on CORE via browser, on WR21 manually).

 

Any suggestions from you on how to fix that issue?

5 REPLIES 5

webiq-sk
Frequent Contributor

Some questions:
1. Are the timezones on the devices setup the same?
2. Does using the Date/Time widget in the HMI and connecting the "Systemzeit" item show the exact same time on both systems?
3. What does the system clock on both devices show? You cannot show this in the HMI
4. Is the affected system using a supported web browser?

reviving for similar issue.

webiq-sk
Frequent Contributor

To receive help on this please answer the questions I posted before. So far it's most often been one of the errors mentioned in the questions which are not WebIQ issues.

CodeShepherd
Community Moderator
Community Moderator

@TiborZ @Mbrue Are ther any news? is this issue still open?

for me, i was able to fix it by checking the local hmi system time.  I have no good way to set up a time server on the core, or to relay a time server from somewhere else to the core, so i have to manually set the hmi system time.  It looks like webiq isnt sending a good T0 marker and is relying on synchronized timestamps (IMO).

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist