FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
06-22-2023 09:41 AM
Hopefully some nice easy questions...
My first use of WR2107 and WebVisu (do not have hardware yet so unable to test before developing screens) and haven't found much documentation so please could you answer the following:
1. WR2107 screen resolution is 1024 x 600 so was going to develop WebVisu screens in same resolution. However do I need to allow for any space for browser frame/window or is it possible to launch browser without border?
2. How would you configure browser to auto start to correct webpage on power cycle?
3. What browser is installed on WR2107?
4. Any other configuration hints?
Many thanks!
Solved! Go to Solution.
06-26-2023 05:23 PM - last edited on 07-19-2023 09:23 AM by CodeShepherd
The panel will come in with a Kiosk app. You can set that up to point directly to the correct ip:port for WebVisu.
If Kiosk mode was running when the device lost power then it will boot back up in Kiosk.
Depending on the software version on the device when it arrives you might need to update it to RC4. You can find instructions for that
https://developer.community.boschrexroth.com/t5/ctrlX-HMI/Info-WR21-Firmeware-update/m-p/76916#M248
Kiosk is a borderless browser for the most part and runs on the chromium engine.
07-10-2023 10:38 PM
link above does not work, I think it's a forum problem; copy/paste teh text brings up the page.
Also, the above link does not have any instructions on how to update the firmware.
07-11-2023 11:25 AM
for me the link is working. I copied it in the browser line..
In the link is not descirbed how to do it because therefore I have to send you the image file and the according manual. This "manual update process" is only necessary for the "old" devices. The devices we currently deliever are able to update themself easily via installed app.