FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-04-2022 03:33 AM
Hi Community,
I am using WR2107 CtrlX HMI,
Using the kiosk setting to set auto launch and lock codesys webvisu webpage when startup.
When i turn on the CtrlX and CtrlX HMI the Webstation app could not refresh the web page. It required Kiosk password to refresh the webpage.
Is it possible for the user refresh the webpage to display codesys webvisu without the Kiosk setting password?
Warmest regards,
Open
Solved! Go to Solution.
08-24-2022 04:18 PM
Hello,
I've got the same issue and no solution instead of switching off/on, any other thoughts?
08-29-2022 02:49 PM
I have this quesiton too. The codesys WebVisu takes to long to boot. Hopefully there is a script that can delay this?
08-31-2022 09:29 AM
09-07-2022 05:19 PM
The idea of a delayed start is quite good.
I don't have any experience with Android, but is it possible to write a .bat - file (or something) which starts kiosk mode as a delayed task action?
With Windows it is possible to create a task with a delay of xxx seconds/minutes
12-19-2022 09:53 AM
Hi,
I have the same issue. At the moment we will delay the start of the HMI until the CtrlX Core is in Run mode.
Still, is there any chance it will be solved by the app in the future ?
01-31-2023 10:35 AM
Hi.
Is there any info on possible fix for this issue in the future? Or maybe has somebody done some kind of work around solution?
02-08-2023 04:36 PM
According to RM22.11 presentation "Starting Bugs" were eliminated and the possibility to get the newest releases.
Is this issue about starting time and kiosk mode not updating IP part of this bug solution?
02-28-2023 07:36 AM
At the moment there is no new feature fixing this problem but we are working on this with the supplier. Unfortunately I cannot tell you any date for this.
02-28-2023 08:16 AM
Good morning,
So which were the "eliminated starting bugs"?
07-25-2023 05:20 PM
was this issue about starting in Kiosk mode fixed? is there any solution for this?
Thanks
07-26-2023 12:43 AM
Here is a workaround.....
Workaround for delaying startup of HMI on WR panel... (boschrexroth.com)
I haven't tried it yet.