05-06-2020 07:40 AM
Has it been considered to implement an automatic recalculation of settings via FWA when you change units? E.g. mm/min --> mm/s
regards,
Stefan
Solved! Go to Solution.
05-07-2020 04:30 PM
Not in the first step of the ctrlX DRIVE Runtime
05-11-2020 01:54 PM
It´s a pity, it would be a nice feature for new customers. So do we still need to provide a boot up sequence if we change from mm/min -> mm/s as up to now, if resolution is changed once after first boot up?
05-14-2020 10:46 AM
No, it should have been good enough to just shortly go to OM mode and back again to PM. Then the new scaling should have been taken over. A reboot is not necessary. With the new CM mode this now might get more transparent.