FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-03-2020 02:22 PM
Which reaction will the ctrlX DRIVE do when the positive or the negative power limit (from/to DC Bus) will be reached ?
Is the current and/or the velocitiy then limited ?
regards, Stefan Sv.
Solved! Go to Solution.
09-07-2020 08:09 AM
If we are at the power limits the torque will be restricted.
10-20-2020 05:32 AM
What about current and speed?
10-23-2020 11:53 AM
Current is related to torque or force and will therefor be reduced as well. The speed normally will not be affected only of course if the torque/force drops as reaction the speed may drop as well.
10-23-2020 03:07 PM
THX! It's very useful for me!