FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-17-2023 09:33 AM
Hello,
i would like to update my ctrlX Core ("standalone" Core X3 at the moment V1.18) to V1.20. In my application i have a XVR, two XMS and three XMD all with the Firmware "AXS-V-0308N-NN.03"
In the release notes from the V1.20 i found a table (3.1.2) wich says that if i have a drive wiht a integrated Core that it is necessary to update the firmware of the drive to AXS-V-0316 or AXS-V-0402 ...
Does this also apply for the Standalone core or only for the ctrlx-Drive Plus/ Drive integrated core?
Regards
Max
Solved! Go to Solution.
11-17-2023 10:02 AM - edited 11-17-2023 10:02 AM
The current hard link between ctrlX CORE and ctrlX DRIVE runtime only applies to the drive integrated combination as there it needs to fit to each other.
A standalone ctrlX CORE can have versions independent of ctrlX DRIVE (or 3rd party drives) connected to the EtherCat. We recommend to have the same runtime on all drives in a machine but it is not a must.