01-16-2024 03:17 PM
If XMS does not use XVR, can it be powered by an external DC power supply? If possible, is there anything special to pay attention to?
Solved! Go to Solution.
01-17-2024 09:49 AM
All XMS, XMD and even XCS or XCD can be powered by an external DC bus voltage power supply. Mind that you may need additional components like
- mandatory DC bus capacitances XLC to smoothen the DC bus voltage (--> 47 μF needed per kilowatt [kW] of continuous power)
- mandatory DC bus adaptor XAS4 to connect the 3rd party DC bus power supply unit to the ctrlX DRIVE package --> note the specified limitations in the manual
- DC bus chokes XLL to balance the current if needed
- additional Y capacitances to avoid floating DC bus voltage to ground at XE if needed
For XMS and/or XMD just set the following parameters:
For XCS and/or XCD set the following parameters additionally to the ones for XMS/XMD:
01-17-2024 09:56 AM
Thank you for your reply.