XCS2 with 120Vac single phase

XCS2 with 120Vac single phase

GustavoTaffarello
Established Member

Hello dear community members,

We've just got few ctrlX DRIVE demo kits from Germany (pn: R911418966) and I am wondering here if there is way to move the axis from bb to Ab with 120Vac as the mains single phase.

The drive has AXS-V-0404 firmware and I am trying to have the Ab as soon as it jumps to OM (with DC Bus charged).

I can see that the mains peak voltage feedback is there, but the mains frequency (S-0-2016) remains at 0Hz. I have also tried using the IOs at the XG31, but no success.

Should I force some "reserved" bit somewhere? Are other parameters (like P-0-0860) that I should force just to test here in Lab? No high speeds and no load.

I am also attaching the parameter file here.

GustavoTaffarello_0-1699029122870.png

GustavoTaffarello_1-1699029218966.png

 

1 REPLY 1

Drives_Uwe
Community Moderator
Community Moderator
Unfortunately this is not possible. Use a power supply device in order to create a 24 or 48 V DC voltage. Then you can make the ctrlX DRIVE amplifiers work in inverter mode. Set DC bus voltage threshold to 20 or respectively 40 V. Set P-0-0118 Bit 15 to „1“!
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist