FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
12-11-2023 09:23 PM
Hello,
When using the ML3 linear motors with XCS2 does it need mains voltage of 400VAC or is 480VAC ok?
Can ctrlX DRIVE, via parameter P-0-0853, limit the DC bus to 540 Vdc?
Thanks.
Solved! Go to Solution.
12-13-2023 10:50 AM
Maximum DC-bus voltage for ML3 motors is 600V
So 480VAC is not possible with XCS2 as you wil have 680V DC bus voltage
It is not possible to limit the DC-bus voltage with the mentioned parameter P-0-853. The value must be bigger than 1.08*P-0-0815. The DC-bus voltage is a direct result of the input voltage-