Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Velocity Data - Time Unit not accepted in Linear

Velocity Data - Time Unit not accepted in Linear

Pinball_NL
New Contributor

In the ctrlX drive I like to have the scaling in mtr/s andor mm/s^2.

I get an error message when changing the scaling from min to s.

Pinball_NL_0-1687768455777.png

Above its in Degrees. Then its accepted. But if you cange over to Linear this error pops up.

IDN not supported!

Pinball_NL_1-1687768620544.png

I test this in 03V08, but at the floor we should have 03V16. But I will check that. 

Is this a known thing? Now I  have to use a speed of mm/min

2 REPLIES 2

Drives_Uwe
Community Moderator
Community Moderator

If set correctly it should be possible to set the units to e.g. m/s. Using what firmware version shouldn´t matter. See:

Drives_Uwe_1-1687842612266.png

 

Drives_Uwe_0-1687842586216.png

 


If you need further help send your parameter file in format "all parameters" for detailed check.

Hello Drive_U

If I change it in the "scaling extended" view then it is accepted and changed.

Pinball_NL_0-1687850504735.png

After that its also changed (and accepted) in the default scaling dialogue.

Pinball_NL_1-1687850626057.png

 

 

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist