FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
02-27-2023 10:34 AM
Hello,
We have a customer that is using the ctrlX Core with seven ctrlX Drive,
This customer is used to work with B&R and he claims that they have a tool to calculate the drive and motor diagram and also the cycle points, so he can check if the mechanics and the drive and motor are accordingly sized,
I know that with the IndraSize we can do it offline but whit this tool they can do it connected to the real machine and with the real cycle points,
So, do we have something similar to this?
Thanks,
Solved! Go to Solution.
03-07-2023 06:01 PM
A look on the behavior of the mere motor drive combination inside the ctrlX DRIVE Engineering tool is possible, see (one can look on the torque or power over speed characteristics over the complete speed range):
To check as well the application cycle one needs to
- create a scope file
- export this scope file to Excel (".csv"-file)
- insert this file into the sizing tool IndraSize
- and check the working points
See:
03-14-2023 10:19 AM
Many thanks 😊